Part Number: ADS1256
Hi Chris,
I wonder if op amp buffering for the ADS1256 input is necessary and when do we use it for optimal performance
Thank you,
Khoi Ly
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1256
Hi Chris,
I wonder if op amp buffering for the ADS1256 input is necessary and when do we use it for optimal performance
Thank you,
Khoi Ly
Hi Khoi,
You are referring to the ADS1256's internal input buffer, correct?
Enabling the ADS1256's internal buffer increases the input impedance of the ADC, is also causes a slight increase in noise. It is needed when using high-output impedance sensors, as the sensor output-impedance will interact with the ADC's input impedance and form a voltage divider (i.e. gain error). Unless your input source is already buffered, then I would usually recommend enabling the internal buffer.