This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J60EVM: ADS54J60EVM

Part Number: ADS54J60EVM
Other Parts Discussed in Thread: ADS54J60,

HI 

I really do enjoy my ADS54J60 as it works great! I have a problem though. Using the HSDC Pro GUI it will turn "dead" if I leave for 5-10 minutes. 
If I keep on capturering data it will stay "alive". I have always been able to make it work agaian loading the file ADS54J60_LMF_8224.cfg.

I also use the Autamation SW that was included in the delivery. I am able to control it using a cpp application based on the example provided.
But same thing happens - the system stops if I leave it. And as far as I can see there is no way to reload the file ADS54J60_LMF_8224.cfg using
SW. I have to do it manually. (Using Write_Registers_U32 doesn't work either!)

First question is: "Is there something wrong with my ADS54J60EVM"?

Second questio: "If not - is there a way to restart from SW"?

Thankful for any comment! /Jan Wennström