Other Parts Discussed in Thread: TPL0102-100, MSP-EXP430FR2355,
Hi, I have tested this Op Amp gain controlling application using an analog potentiometer and I saw the changing gain using an oscilloscope.
Instead of using an analog potentiometer, I want to use a digital potentiometer to control the gain of a signal.
1. From this example,
What is the range of V_I? Can I apply 40V to the High or Low terminal pins?
I couldn't find this from the datasheet.
2. Just like the first picture, I was thinking of shorting the wiper terminal to the high or low terminal.
If I do this, can I control the resistance(high terminal - low terminal) from 0 to 100k Ohms?
I used other digital potentiometers but those didn't work when I shorted it.
Instead of the first application, I want to use this digital potentiometer to control the gain.
If there is an alternative way instead of shorting the two terminals, I wish to hear about it, please.