This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS4246EVM
We are using the ADS4246EVM connected to a Xilinx Artix-7 FPGA as a development system whilst our hardware is ready.
As a medical company, we need to make sure the ADS4246, via the SPI, has been programmed correctly. Therefore, after programming the ADC, we read back all of the registers from Address x01 (After setting READOUT in Address x00 first) to make sure the SPI registers are correct.
However, when reading address x4A, I see bit 4 high (so Data Out = x10) instead of the programmed x00.
Is it:-
* The SPI Address was incorrect (so not x4A)
\=> However have reduced the SCLK vastly, and still seeing bit 4 still high,
* The ADS4246 or the datasheet is incorrect
\=> The datasheet is from 2013, so very unlikely
* Part of address x4A (and other registers?) are internal test values
\=> So mask the data coming the ADC so only the right parts of the registers come through (i.e. Mask any bits that say 'Always write 0' in the datasheet)
* A.N.Other?
See attached 'Scope screenshot of the SCLK and SDOUT of Address x4A.
Many thanks,
Tim
> It was a little hard to understand your last message, but if the data sheet mentions to always write a "0" to a particular bit location, then make > sure you are doing this.
I am doing this.
Example:
Address: x4A, Writing: x00 (See attached x4A register in the datasheet)
Reading back: x10
Something is not correct, is it?
Tim,
When you wrote the following:
Tim Wells replied to ADS4226EVM: SPI Issues when accessing through a FPGA.
Jim,
This has resolved itself - when we soldered some flying leads to the SMT Buffer chip (1.8V SDOUT => 3.3V SDOUT), it started working. Thanks!
Tim
I thought all was well. Is this not the case?
Regards,
Jim
Tim,
You should only be concerned about the ‘programmable bits’ the datasheet gives for a register address. Other bits in a register address are sometimes shared with internal trim registers. Since the trim can be different from part to part, these shared bits may read back as either a "1" or "0" depending upon the trim value of the device. Bit 4 in register address 0x4A is one such bit. What you are reading back is expected.
Regards,
Jim