Part Number: ADS1256
I have ADS1256 ADC module, which is interfaced with a STM32F746,
I stared with a Read Registers default values are ok as per data Sheet but when i write any value to any register MSB i.e bit7 is always '1' while reading,
for eg.
DRATE: A/D Data Rate (Address 03h)
if i write a 0x33 that is 00110011---15SPS
while reading i always get a 0xb3 that is 10110011,
similarly for all register read bit 7 is always '1'
please find the attached logic analyzer Screen shots
Thank you.