Part Number: ADS1262
Hello
I have a question related to the differential input range of the ADS1262.
I have a system where it is used a load cell of 100kg with a Wheatstone bridge configuration. It is excited with Vexc(+)=5V and Vexc(-)=0V (GND) and it has a sensibility of 2 mV/V; so the differential output of the load cell is:
- (10 mV) when it is applied a traction effort. In the output terminals there is a voltage aprox. of IN(+) = + 2.5V and IN(-) = + 2.49V.
- (-10 mV) when it is applied a compression effort. In the output terminals there is a voltage aprox. of IN(+) = + 2.49V and IN(-) = + 2.5V.
Connected to the load cell in ratiometric connection is the ADS1262. The ADS1262 is supplied with AVDD=5V and AVSS=0V, and VREFP=5V and VREFN=0V. If it is programmed a gain for example of 32V/V, the differential input range of the ADS1262 is of ±156mV. And the question is, why the ADS1262 can measure a negative differential input signal, as the - 10mV, if it is supply with a positive signal (AVDD=5V and AVSS=0V), that is, of unipolar way? Is not it supposed that supplying in a unipolar way should only be able to read positive values in the input?
Best regards.