This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DAC81416EVM: Power Up the DAC81416EVM

Part Number: DAC81416EVM

Tool/software: Linux

Hi,

 I have a DAC81416EVM board and would like to test SPI communication.

I have connected the J8 pins for SPI communication as follows:

J8.2 CS

J8.3 MISO

J8.4 MOSI

J8.5 3.3V

J8.6 GND

J8.8 SCLK

I have no idea if the device is up and running or not since I do not see any power led indicator on the board.

What is the minimal requisite to power up the device ? Do I need to power the VCC on the J7.7 pin ?

Thanks

I