Part Number: DAC37J84EVM
Other Parts Discussed in Thread: DAC38RF82EVM, TSW14J57EVM
Hi All,
I am trying to interface DAC37J84EVM with the Zynq Ultrascale + and I need help
My approach & initial setup:
L = 8
M = 4
F = 1
K = 20
S = 1
Line rate = 7.3728Gbps
Reference clk = 184.32
1) Vivado block Diagram is shown below:
data for all signals / samples:
assign signal0_sampl0 = 'h7530;
assign signal0_sampl1 = 16'h0001;
2) I configure JESD interface in microblaze by programming registors via AXI as follows:
Xil_Out32(ADDR_start+0x004, 0x1); //RESET IPCORE
Xil_Out32(ADDR_start+0x008, 0x1); // Support ILA - ON
Xil_Out32(ADDR_start+0x00C, 0x0);// Scrambling - OFF
Xil_Out32(ADDR_start+0x010, 0x1);// Sysref - ALWAYS
Xil_Out32(ADDR_start+0x014, 0x3);// Multiframes in ILA = 4
Xil_Out32(ADDR_start+0x018, 0x0);// Test mode = Normal operation
Xil_Out32(ADDR_start+0x020, 0x0);// Octets per Frame F=1
Xil_Out32(ADDR_start+0x024, 0x13);// Frames per Multiframe K=20
Xil_Out32(ADDR_start+0x028, 0xFF);// Lanes in use = 8
Xil_Out32(ADDR_start+0x02C, 0x01);// Device subclass 1
Xil_Out32(ADDR_start+0x80C, (L << 24));// L = 7 (Number_of_lanes -1), DID = 0, BID = 0
Xil_Out32(ADDR_start+0x810, (CS << 24) |(N1 << 16) | (N << 8)| M );// CS = 0, N' = 16-1, N = 16-1, M = 4-1
Xil_Out32(ADDR_start+0x814, (HD << 16) );// CF = 0, HD = 1, S = 0, SCR = 0
Xil_Out32(ADDR_start+0x818, 0x0);// 0x818: RES1 = 0, RES2 = 0
Xil_Out32(ADDR_start+0x004, 0x1); //RESET IP CORE
NOTE: I read the regisrets back to make sure that they are correct.
3) I program the FPGA and Microblaze
4) I program DAC via USB (DAC EVM GUI)
5) I reset JESD & trigger sysref
6) In the alarm window only DAC PLL is not locked. I don't see any other alarms and I cant see anything on the (oscilloscope / spectrum analyser).
I connected clocks to LEDs. They blink as expected (after clock divider).
I am not sure how to start debugging the DAC37J84EVM JESD interface.
Any suggestions?