This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: ADS1298 big interference and steps

Part Number: ADS1298

Customer encountered several problems when using ADS1298. Please give  some suggestions. The problems are as follows.

1.In July 06, 2019, a total of 187 people were tested in the company. Half of them had problems of big interference and steps.

Appendix is the waveform with larger interferenceADS1298 noise.docx

2. In production debugging, ADS1298 input connect to GND, and then test the output. It is found that some chips have high interference noise.

3. Because of the poor uniformity  ,They hope that every chip manufactured will test noise, test time 10-20s, output noise amplitude < 3uVpp, minimum CMRR > 110dB.