Hi Folks,
first of all, I forget to collect forum links about this questions, but seeking on the net, I have found several pages and questions:
why developer is not necessary to use external amplifier at the input of ADS1299???
As I calculate it, (ECG signals around 1 mV, EEG signals 10uV, fetal ECG should be same as EEG, and so on...) using the maximal gain, the input range is around 200 mV. It is far less then the signals in interest.
- So if I want all of the 24 bits for data representation, why I cannot use external amplifier stage?
- I using it, should I use the SoC BIAS amplifier output as DRL, or should I use an own?
- What should be the reference of the ADS1299? Connecting the SRB1 to GND, BIAS etc?
Regards,
Norbert