Part Number: ADC31JB68EVM
Hello,
I am looking for some help. I am using the ADC31JB68EVM in conjunction with the TSW14J56EVM. I have modified the ADC31JB68EVM for clock multiplier mode (PLL2 Only) by installing a 100MHz XO at Y3 and following the configurations required in section 5.1.1 of the ADCEVM user guide. I have also installed C51 and C67 (0.1 uF). I have configured the LMK on the ADCEVM to produce a 100Mhz clock on DCLKout8 (FMC_FPGA_DEVCLKA, FMC pins D4,D5) The issue I am having is the TSW14J56EVM D4 does not blink (Indicates presence of device clock from ADC EVM when blinking). The FMC_FPGA_DEVCLK pins (D4,D5) of the FMC connector on the ADC31JB68EVM are outputting the signal below.
Can you recommend any trouble shooting ideas for identifying why the TSW14J56EVM is not recognizing the device clock?
Thank you.