Other Parts Discussed in Thread: ADS54J54
Hi,
We just received a ADS54J54EVM (PCB REV C). I connected the 5V supply and USB and ran the GUI. Then I downloaded the “ADS54J54_500M_442.cfg” configuration file (actually went through all the steps in the EVM’s user guide and GUI does have connection to the EVM). None on the 4 LEDs connected to LMK is illuminated and all the LMK outputs seem to be silent. Is it supposed to work without any other modifications to the register than is done by the config file? Do I have to change any of the configuration jumpers or anything like that? What is the default clock configuration according to the config file I mean PLL1 locks to what and PLL2 locks to what (MUX positions, enables etc)?
Regards/Ramin
PS. I just checked Y2 (100MHz VCXO) and its completely dead, even though Jumper J6 is on. Any advise?