This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8580: DAC8580IPW. Broken Device . Output-pin wave is incorrect.

Part Number: DAC8580

Please confirm attached-file.  (Microsoft word file)

Texas Instruments_english 20191031.docx

  • Hi,

    Can you please clarify the following:

    1. Is the error transient at device startup, or are you writing to the device?

    2. Can you provide a screenshot of the communication to the device that results in the error transient?

    3. Can you monitor the reference voltage as the error transient occurs?

    4. Does the device recover after the transient? Can additional inputs be provided to the device? 

    5. Are all the digital input pins stable during the transient? For example, does the value of OSR1, OSR2, RESTB, BPB, and MUTEB change before or during the transient?

    Thanks,

    Paul

  • Any updates?