Other Parts Discussed in Thread: ADS7882, ADC0820-N, , ADS7886, ADS7040, ADS8371
Curious to know if this is a supported thing to do. Does tying /RD low satisfy the requirement of the "dummy read" necessary to auto-config the device for 3V operation? Will the conversion result appear on the data pins after /CSTART if /RD is tied low the whole time? Or must /RD be pulsed as in the timing diagrams?
I'm basically looking for a 3.3V device that can operate in a mode similar to the TI ADC0820-N's "RD Mode," wherein all other control signals can be tied (to appropriate levels) and one need only toggle the /RD signal to both initiate a conversion and receive the result. The TI ADS7882 is a near miss, as it requires 5V, and I'd like to avoid having to find (or create) 5V someplace.
All thoughts / suggestions much appreciated!
Very best,
Aaron