Hi,
The datasheet for the TLV571 states that the control registers are set at power-up, and latched at a rising -WR edge. Since there are two control registers, am I to assume each of the control registers are set separately, and they are held internally until -WR and -CS are asserted, at which point they are latched?
For example, would the following steps be correct:
1. Set A1:0 = 00, and set D5:0 pins accordingly.
2. Set A1:0 = 01, and set D5:0 pins accordingly.
3. Assert -WR and -CS to latch both registers internally.
Assuming this is correct, does this mean that the control registers cannot be changed without a reset?
Regards,
Sahil