Other Parts Discussed in Thread: ADS1198
Hello.
I want to use ADS1198 and ADS1194 as 12ch input.
I don't use WCT, GCT, RLD, PACE, GPIO.
(Input Conditions)
[Power Setting: AVDD = +1.5(V), AVSS = -1.5(V), DVDD = +3.3(V), DGND = 0(V)]
[External References: VREFN = AVSS, VREF = VREFP - VREFN = +2.5(V)]
[Input-Signal: AINN = 0(V)( =AnalogGND), VIN = AINP-AINN = AINP]
I have the following questions.
<Question>
1. Are IN8 ~ IN5 (No. 1 ~ 8) of ADS1194 connected to AVDD (not OPEN)?
2. Are NC(No. 27, No. 29) OPEN?
3. Are GPIO 1 to 4 connected to DGND?
4. Is RLDREF(No. 60) OPEN?
Connect a CR (1500pF, 1MΩ) filter between RLDINV (No. 61) and RLDOUT (No. 63) for only one IC.
Another IC opens RLDOUT (No.63), Should I connect RLDINV (No. 61) of both ICs?
I see so it when I watch P.60 fig.52.
※See attachment CONNECTION.pdf.
5. Even if WCT (No.64) is not used, is 100pF connected to No.64?
※See attachment CONNECTION.pdf.
6. Is the power supply connection (AVDD, AVSS, DVDD, DGND) and Input-Signal as shown in the attached figure?
※See attachment CONNECTION.pdf.CONNECTION.pdf