Other Parts Discussed in Thread: ADS1261
Dear All,
Can i post some updates for the problem we faced with the ADS1298 regarding the detection of the pacemaker from the odd channels, which i have discussed it with you before in the topic with link http://e2e.ti.com/support/data-converters/f/73/t/841642.
To make the long story short, we were trying to detect the pacemaker pulse with the the smallest duration and amplitudes (equal and smaller than 10mV - 0.1ms), we were using the same circuit stated on the paper http://www.ti.com/lit/ug/tidub75/tidub75.pdf, but instead of using the SAR ADC ADS7042, we are using the ADS1261, because its higher sampling rate and it has 24-bit high precision ADC, it is needed on our design for the pace detection algorithms and other required functions.
Here is the schematics for the connection of the input stages of the ECG leads to the AFE, taking in your consideration that the PGA of the AFE is set to 6.
After using a noise-free environment to get rid of any unwanted noise, we can easily detect the pacemaker pulses from even channel with 2mv- 0.1ms, as you can from the following picture, this is the plotting for data taken from the pin (TESTP_PACE_OUT) by the ADS1261 without any digital filters, only the anti-aliasing low pass filter, the pacemaker pulses are so clear and can be detected easily by the microcontroller.
We still have problem in the detection in the pacemaker signals derived from the odd channels, it has a higher noise which cover the pacemaker pulses.
this is the signal derived from an analog channel, from the pin (TESTN_PACE_OUT), with 10mV - 0.1ms.
and this is the pacemaker signal with 50mv - 0.1us without any digital filters also.
We only want to know why the path of the odd channels contains more noise than the one with the even channels.
Also this a comparison for the two outputs together without any pacemaker signals, only the ECG outputs, the blue signal is derived from the odd channel, and the even signal is derived from the even channel.
Is there any way to reduce this noise? and do you know any reason why this noise is appeared?
looking forward to your reply, and please don't hesitate to contact me if you have any further details.