This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300EVM-PDK: Hardware circuit question

Part Number: AFE4300EVM-PDK
Other Parts Discussed in Thread: AFE4300

Hello,

I have a question about the hardware circuit of AFE4300EVM-PDK.

In the datasheet of AFE4300, PIN43, PIN44, PIN72, PIN73, PIN74 and PIN75 are "NC", which means "Do not connect". However, in the schematic diagram of the evaluation board, the above PINs are connected, in which PIN43 and PIN44 are connected to test points TP2 and TP3; PIN72 connects with AVDD_OUT; PIN73 connects with SIMO_M; PIN74 and PIN75 are connected to AGND1.

Is there any problem in AFE4300 datasheet or is it not the latest version?

Many thanks,
Haoger