Part Number: ADS1235
Other Parts Discussed in Thread: ADS1261
Hi
First I try to describe our planned configuration of the AD1235. We have an external +2.5V reference on REFP0/REFN0 and also connect this +2.5V to AIN0 as reference input for a single-end measurement.
The input voltage range of our application (single-ended) is 0.35 .. 4.7V and we use the internal PGA with gain=1.
Now my question: Is there a way to get an out of range value (range of our application) back from the AD1235 (e.g. 0x000000 or something else)? We think about a diagnostic function of the ADC to read a defined value from the ADC which is out of the range of our application.
What happens if I connect 0V to one of the inputs and measure it referenced to my +2.5V (e.g. 0V @ AIN5 / +2.5V @ AIN0)? So the differential input voltage would be -2.5V, that means it's out of the PGA range (+0.3V .. +2.2V). what is the result of such a conversion?
I think with a bypassed PGA we could do that, but with the included PGA?
Best regards
Oliver