Part Number: ADS1248
Hi,
Using the ADS1248, I will changing the design to use an external reference instead of the ADC internal reference for both the ADC and transducers (from 2.048V to 3.3V), since the transducers require a minimum reference voltage of 2.5V. I will be leaving the capacitor across Vrefout and Vrefcom in place. Should I make any changes to the pull-down resistors connected to REFP0 or REFN0, since I will now be using the external reference voltage for the ADC? Should I add any capacitor across REFP0 or REFN0? Any other suggested circuit changes that should be made when changing from the internal reference voltage to an external reference voltage?
Thanks,
Saribel