Part Number: ADS1235
Other Parts Discussed in Thread: ADS1261,
Hi
First I try to describe our used configuration of the AD1235. We have an external +2.5V reference on REFP0/REFN0 and also connect this +2.5V to AIN0 as reference input for a single-end measurement.
The input voltage range of our application (single-ended) is 0.35 .. 4.7V and we use the internal PGA with gain=1.
Here the simplified schematics:
Now comes my question:
All measurements where we use the internal VCOM seems to be wrong (e.g. "VCOM-AIN0" or "VCOM-AIN5"). All other measurements get a result as expected.
The internal voltage VCOM is defined as "(AVDD+AVSS)/2", so in our applications it's VCOM = +2.5V.
Is there something special to consider when useing the internal VCOM?
(As example, if we measure "VCOM-AIN0", we expect a converted result of 0V (+2.5V on both PGA inputs => differential 0V), but in real we get a result far away from 0V)
Here are the register settings we used for the measurements:
Best regards
Oliver