Part Number: ADC104S021Q-Q1
IC: ADC104S021Q-Q1 (error parameters DNL=+/-0.4,INL=-0.4...+0.3,offset error=+/-0.4. FSE=+/-0.7)
when ADC104S021Q-Q1 convert an analog singal to ADC,wo can get the typical ADC value,but how can i calculate the max /min value of the ADC;
for example,Vref=5V,input analog=2.5V,then the typical ADC=512,if ADC-max=512+(DNL+INL+offset error+FSE),ADC-min=512-(DNL+INL+offset error+FSE);
then the ADC value will be a decimal?