Part Number: ADS1298
The input channels are getting saturated as I have not using the RC level shifter at each input channels of ADS1298. My reference voltages are AVDD +2.5V and AVSS -2.5V. Earlier I was using a RC level shifter to set the baseline voltage to 1.2V and it was working fine all the time. But when there is no RC level shifter (which gives error in lead off detection) the input differential band goes beyond the reference voltage so getting the values 0xFFFF in all the channel.
Please help me to get the stable (constant) baseline with no RC level shifter circuit.
When all 10 leads are connected to the subject to acquire 12 lead ECG the voltage band for each channel should be within the reference voltage all the time. Please help me to achieve this.
Thanks in advance.