Part Number: ADC31JB68
Other Parts Discussed in Thread: LMK04828,
Hi,
I am doing almost same test with ZCU106 board + TSW14J10(rev C) + ADC31JB68EVM(rev B).
I am using Agilent N5181A signal generator's 500MHz +12dBm output for CLK input.
I had reworked two registers((R44-R45 to R51-R61) to use LMK_ADC_SYSREF(SDCLKout3).
I have modified designs and firmware also, for Vivado 2019.2 & VItis.
But, the link is very unstable and hard to link.
I can get JESD204b linked after tens of reset try.
I got below ramp pattern. Is this correct pattern?
I had exported the raw data as csv file and attached it.
In every 128 samples interval. decrease as -63.
Below is GUI settings.