This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am testing the ADC31JB68EVM with Xilinx ZCU102 board (FMC HPC1).
But I can read only serial S0 data from the JESD204 IP core output data, S1 looks random data pattern.
Also, I found readout data look jumps. I've attached PLL configuration and ILA waveform.
Hi Kiman,
What is the sampling rate that you are using? Have you also tried to use a ramp pattern?
Best Regards,
Dan
Hi Kiman,
I am able to capture data with our data capture card (TSW14J56EVM) with the settings that you have shared. Have you configured the ADC31JB68EVM in accordance with the user's guided?
Can you please ensure that the JESD IP is configured to accept the 2 lanes of data as shown in the ADC31JB68 datasheet page 26?
Also note that the number of frames in a multiframe (K) defaults to 32.
Best Regards,
Dan
Hi Dan,
Here is my configuration for the Xilinx JESD PHY and JESD IP core.
Each lane has output data size is 32 bit and the total data size is 64 bit with GTH reference clock 250 MHz.
Figure 16 seems each lane data is 8-bit and 250 MHz update rate and make a 32bit for 500 MHz.
Default K I used 16 and need to change 32 as you recommended.
Can you please review my configuration, I have a no idea how to set up the LMFS 2111 from the Xilinx JESD IP core.
Hi Kiman,
I don't have much experience with initializing the JESD204B IP core, but most of what you have share looks "ok" to me (other than the K value). I'm also not sure about the LMFC buffer size (currently set to 1024, shown on the first image you shared). I'll have someone take a look to see if we can provide further help here.
I would also suggest reaching out to Xilinx to see if they can offer support on the FPGA side.
Best Regards,
Dan
Hi Dan,
Update:
The Xilinx JESD 204 set Default K = 32, It happened Link error from ADC board and NO serial input from JESD IP.
Thanks,
Kiman
Hi Kiman,
I missed that the frame F is set to 2 in your JESD IP initialization, and it should be set to 1. I think this will correct the link error that you saw in your update.
Best Regards,
Dan
Hi Kiman,
I'm not certain I follow your last question. Do you know what data is missing? Since this is a one channel device, isn't the sinewave being faithfully captured? Are the top two rows, that have the sinewaves, representing both lanes?
Best Regards,
Dan