Part Number: ADS1258
Other Parts Discussed in Thread: ADS1261EVM
Hello
I am likely to use your multi-channel ADC "ADS1258" in my next design.
Now I just want to make sure that I correctly understood the functionality of this ADC.
The ADC would have a 5V analog supply and a 3.3V digital supply voltage.
Let's assume that I will have to measure 10 sensors, each with an output signal between 1.45...1.55V.
The sensors have a supply voltage of 3.0V.
I would use the single-ended Auto-Scan Mode and provide 1.50V to AINCOM (Accurate 1/2 voltage divider from sensor supply)
This way the differential voltage at MUXOUT will be -0.05...0.05V right?
With an external amplification circuit (like on page 45 of the datasheet but with Gain=20) the differential ADC input voltage would than be -1.00...1.00V.
So I would scan the 10 sensors and measure voltages with the ADC between -1.00...1.00V on each channel. Is this correct?
With the reference set to 3.0V -> 1LSB = 381.5nV this corresponds to -2’621’440...2’621’440LSB reading (two's complement already considered)
An additional question:
Do you see problems with USB operation? So I would supply the ADC with 5V bus voltage (maybe filtered with a LC-filter) and generate proper and quiet 3V with an LDO and some extra filter effort for the Sensor supply and ADC reference.
Please let me know if I misunderstood something or if you have anything to mention.
Thank you very much!
Regards,
Sandro