Part Number: ADS1292R
Other Parts Discussed in Thread: ADS1298, ADS1292
Hi
Thanks to the great support from this forum especially Mr Alexander Smith, Mr Ryan Andrews, Mr Tom Hendrick and Mr Collin Wells, the program is now converting the output codes back to EMG voltage successfully. Now, since the software part is almost complete, I am planning to optimise the hardware part. The schematic of ADS1292R to acquire EMG signals is shown below.
The following are the important points:
1. 3.3 V for both digital and analogue supply
2. RLD input for the reference potential
I have a few thoughts that require some clarifications
1. I have read that RLD can be sourced from the inputs (int this schematics 1N and 1P) and the circuit is as shown below:
This seems a better approach. So using a capacitor and a pull-up resistor I can provide body reference to the IC. This is adapted from the ADS1298 datasheet. Can this be applied to ADS1292R?
2. If it is possible, what is the theory behind it? (in short, could anyone explain to me why this works?)
3. To convert the output codes to voltages, I use an internal reference (2.42 V). Does adopting this RLD configuration affect the reference voltage? ( I think the reference Vref is for ADC and RLD is for the amplifiers)