Other Parts Discussed in Thread: CC1310, OPA192, ADS1282, ADS8685
Dear TI Team,
I need your help/Review to correct the attached TINA Circuit for Geophone amplifier. I am not analog hardware expert, have basic knowledge. In attached circuit, have used information from this blog as well from web. I need to design a geophone sensor amplifier using HS-6, 10Hz, possible to extend the range to lower side till 100mHz to 1Hz using electronic methods, e.g. NVIC or any suitable method. The OPA192 and ADS8924B are planned for amplification and ADC. I have attached documents - data sheets of Geophone, document to derive the transfer function of Geophone and TINA simulation circuit. The unit will powered by 5V battery using LDO with 7.2V Li-Ion Battery. This signal amplifier will be connected to CC1310 module to send the data. The use of external ADC is needed, max use of freq will be 250Hz.
1. Does placement of RC filters after each stage of amplifier needed?
2. Anti-aliasing Filter (3rd order) after amplifier is good or need to insert between both gain stages?
3. Selection of parts are OK, with 16 Bits ADC measurement?