Part Number: ADS1292R
Other Parts Discussed in Thread: ADS1292,
Hi, I am almost done with my project. Have two questions:
1. When I studied the datasheets of ADS1292 and the evaluation board, I found that in certain circuits (see the figure 1 as an example) two capacitors are connected in parallel with a significant difference in capacitance value. Hence, I designed the schematics (also shown in figure 2) by removing the smaller capacitor as the bigger one allows for some tolerance. Is it the right approach? Or the two parallel capacitors have any purpose? (eliminating the capacitor helps in miniaturization).
Figure 1:
Figure 2
The smaller capacitors are removed.
2. I read (I don't remember the source) that the ADC of ADS1292 has inbuilt digital filters that can eliminate frequencies according to the sampling rate. (For example, If I sample at 1KSPS all frequencies above 500 Hz will be eliminated) Is it okay if I use a 1KSPS for a cut off frequency of 500 Hz since the simple antialiasing filter with a bigger roll-off will allow some frequencies to pass? Currently, I am planning to use 2KSPS for 500 Hz to prevent aliasing. If this is the case, I can sample at 1KSPS. Also, is there a notch filter in the ADC at 50 Hz Fc?
Thank you in advance