Part Number: ADS8556EVM
Like in the related question, the "BUSY/INT" signal of the ADS8556 (16 bit) stays high, when I a set "CONVST_A" to high. However it never goes back to low. Since my controller waits for it go back to low, it is stuck.
The related question does not really provide a solution, besides tying the analog inputs to ground.
I have an ADS8558EVM (12 bit) here, too, and I see the same behavior, so I assume it has to do with the test setup or configuration, since a few years ago I worked with the 12 bit version of the chip and was able to use it.
Settings (hardware + serial):
SW1.1: 0
SW1.2: 0 (4x)
SW1.3: 0 (hardware mode)
SW1.4: 1 (serial)
SW1.5: 0 (refbuf enabled)
SW1.6: 0 (no daisy chain)
SW1.7: 1 (serial A enabled)
SW1.8: 1 (serial B enabled)
SW1.9: 1 (serial C enabled)
SW1.10: 1 (internal reference enabled)
JP1/2/5/6/7/8: 1-2
JP3: 7-8 (FS/CS - J1.7)
JP4: 2-3 (3.3V)
JP9: 1-2, 4-5 and 7-8 (CONVST - J4.17)
JP10/11: 2-3 (+/-12V)
JP12: none
Voltages measured:
TP1: -12V
TP2: +12V
TP3: 5V
TP8: 0V
TP16: 3.3V