Hi Sir,
I'm using ATSAMD51 controller with ADs1015 interface.
power supply to ADS1015 is 5.5 V.
Analog input channel 3 : 2.3V
write config register setting value : e103 . ( adc channel : 3, single ended inputs,+/- 6.144,128SPS, single mode, OS enable)
After reading the config register value : 8583 (default value).
Because of this default value, we can't able to measure the channel input voltage.
Kindly give the solution for below mention points,
1. Why the config register value has always default value ,when config register value (e103) written successful in ADS1015? .
Thanks & Regards,
Poovai Anitha.L