Other Parts Discussed in Thread: USB2ANY
Ref : https://e2e.ti.com/support/data-converters/f/73/t/890391
Dear AK,
In continuation with the above thread, I have replaced a new DAC chip, and still the output not being observed.
I have tried with both the internal and external reference voltage options.
As you mentioned in the last message, I have checked the status register. The value is FF. That is Alarm is set.
I have verified that the Gain = 1 (BUFF-GAIN = 1, REF-DIV = 1).
Still the current drawn by the chip is 300 mA, which means the output stage is not enabled.
I am not sure what I can check further. Do you have any option alternate to USB2ANY ( I do not have one) to check with the example?
I do not find the Labview vi sketch being shared with the example package. Can you please share the vi project of the example so that I can verify the sequence being executed?
This will give some idea to me.
Chandra