Part Number: ADS1299
Other Parts Discussed in Thread: TINA-TI
Hi
I am trying to calculate skin to electrode impedance using 6nA current at 31.2hz generated internally of a single electrode connected to negative end of the 8th channel and positive end is connected to bias electrode.
I have connected an anti aliasing filter(2.2K ohm and 1nF) at the input. My configurations are -
LOFF_SESN -> 0x80.
LOFF -> 0x02
gain is 24 and data rate is 500sps.
when i add an additional 660K ohm resistor at the input the digital output does not change and comes to be 1-2 mV. Shouldn't it be a minimum of 3.6 mV ((660K+2.2k)*6nA)?