Part Number: ADS1115
Other Parts Discussed in Thread: ISO1540,
I am using he ADS1115 behind an I2C isolator ISO1540. I am getting intermittent zero results. I am using a scope to verify the I2C signals, and all looks good.
I have had this issue with several applications so far. My current solution is to read it multiple times to get a non-zero value. Sometimes it returns with data on the first try, sometimes not after 20 consecutive readings.
My application is using an ST STM32G4 controller, but I have had issues before with Arduino test systems. The microcontroller side is 3.3v and the ADS side is 5v. My ADC voltage is close to 5.0V, but not near the 5.5V limit.
While I am sure the part works well, it won't in my applications.