Part Number: ADS7828
Other Parts Discussed in Thread: OPA320, INA331
I have an instance where an ADS7828 device appears stuck in a state where it is giving an erroneous digital output for the analog input.
Here are the details:
-
CH3 of device is connected to output of a pressure transducer.
-
Measured DC voltage for CH3: 0.24V.
-
CH3 is selected by this I2C write command: 0xD4
-
Single-ended inputs
-
C2:C0 = 101
-
PD1PD0 = 01 – Internal reference off and A/D converter ON
-
-
Resulting read value = 0x05AD (1453)
One reason this is suspicious is that this board connects the output of another identical pressure transducer to a 4 channel ADC:
-
Measured DC input voltage: 0.25V
-
Resulting digital output = 0xCD (205)
Given the state of the system when the conversion is done, this result from the 4-channel ADC is what we expect, and we are trying to understand the discrepancy between the ADS7828 result and the 4-channel ADC result.
I can provide data from the other channels of the ADS7828 if needed.