Part Number: DAC5681Z
Hello,
We have a problem for understanding of the relationship between the input data rate (input clock 250MHz) of FPGA and the sample rate of DAC (1GHz) with interpolation. We saw the example provided by the datasheet (page 20 and 21), we understood that the ratio between these two parameters (input data rate of FPGA and the sample rate of DAC) should be 1/4 to have a transition from 4 parallel samples to 4 serial samples without interpolation. What if we apply x2 or x4 interpolation in the DAC ? Should we keep the same ratio 1/4, or change the ratio to 1/8 (x2 interpolation) or 1/16 (x4 interpolation) ?
Thanks in advance,
BR,
Enrique