Part Number: ADS5407
Other Parts Discussed in Thread: ADS54J64, ADC12QJ1600, ADC16DX370, ADS4449, ADC31JB68
Hello,
Please, read the previous questions and answers related to the ADS5407.
So, we plan a 4,000-Channel, 14-BIT, 500MHz ADC system with simultaneous sampling.
I'm looking for the best part with respect to noise levels and power/channel.
Our limitation is that we can't do more than 6Gbps on the JESD204B serial interfaces.
Questions:
Is ADC31JB68RTAT the best part for the job?
Is this a true one-channel 500MHz ADC, and is not made up of two inteleaved ADCs like the ADS5407?
Can it work simultaneously on a 8ns clock supplied to all 4,000 Channels?
Is this a new part that was not available in 2018?
Thank you very much.
Best regards,
Mircea