Part Number: DDC112
Hi. On two different DDC112 chips, I am using external capacitor values of 1000pF and 470pF. According to the data sheet, these should give us full scale currents of 3.93uA (1000pF) and 1.848uA (470pF). Our integration time is 0.001s, so our respective charges should be 3932pC (1000pF) and 1848pC (470pF). I know these values are above what the original datasheet specifies, but in the application notes (sbaa027), it says it is possible to use the higher external capacitors and higher charges if used in the right way. We are staying well below the 750uA threshold stated in the application notes.
What is occurring is we are seeing incorrect current measurements when the input current exceeds ~50% of the full scale currents. When this happens, we see some ramping up of the voltage seen at the input pin, as if more current is being pulled through right before a measurement is taken. This is consistent with the reported measured currents as they start to be 8-15% higher than what we are providing. We are using a constant current source, and were wondering if maybe this current source could be causing issues. This set up is actually for a test stand of ours, and as far as I know, we haven't seen any issues with current measurements in the field. We may not have seen any issues in the field however because we might be staying below 50% of the full scale current for each capacitor.
Let me know if you have any ideas.