Part Number: ADS8684
I have design a board using the TM24C19X. after power the board up (default setting for the ADS8684) I follow the manual data acquisition steps as per spec (pg 84) toggle CS between events .
1) write MAN_ch1 (32 clock cycles) read sample N from previous conversion
2) Write NOP (000) 32 cycles to retrieve the converted channel 1
I have to add an addition write NOP to get the converted data - data is right though
Question: why do I have to do the addition NOP write and two spec pg 34 (data acquisition example) seems to imply I can do it in one 32 clock cycles.
is there a simple code splice (not the Linux version) for this chip?