Part Number: ADS1191
Other Parts Discussed in Thread: ADS1298
Hi Ryan Andrews,
You helped me on solving DC bias related issues. Now I'm trying to make the DC Lead-off detection working in a new project for the same input circuit shown below
The register were programmed as following:
03h LOFF = 0xd0; //bit7:5 tried with different thresholds 000-111 with no difference; bit4: must set to 1; bit0: 0 for DC detect
07h LOFF_SENS=0x03; // FLIP1=0, LOFF1 N&P=3
The LOFF_STAT register would flip the IN1N_OFF and IN1P_OFF bits randomly regardless of the lead actually having contact or not. The status bits in the input data stream behaved the same.
Is there anything I missed in order to make the DC LOFF detection work properly?
Thanks,
Jim