Other Parts Discussed in Thread: ADS8350, ADS8354, ADS8900BEVM-PDK
Hello,
I just got the ADS8350EVM-PDK today. Downloaded SBAC130A.ZIP and performed install on freshly set-up machine with Win10 Professional / 64bit. Was running the install as administrator.
Installation completes to the point when drivers are being installed and this is the moment where the process seems to break:
Running dpinst depending on the underlying platform We are on a 64 bit OS. CreateProcess succeeded INFO: Option set: dumping log info to console. INFO: Current working directory: 'C:\Program Files (x86)\Texas Instruments\ADS8350evm\SDCC Driver' INFO: Running on path 'C:\Program Files (x86)\Texas Instruments\ADS8350evm\SDCC Driver' INFO: No valid 'dpinst.xml' file provided. INFO: Install option set: legacy mode on. INFO: Found driver package: 'C:\Program Files (x86)\Texas Instruments\ADS8350evm\SDCC Driver\NSC_USB-WV5.inf'. INFO: Found driver package: 'C:\Program Files (x86)\Texas Instruments\ADS8350evm\SDCC Driver\TI_USB-WV5.inf'. INFO: Preinstalling 'c:\program files (x86)\texas instruments\ads8350evm\sdcc driver\nsc_usb-wv5.inf' ... INFO: ENTER: DriverPackagePreinstallW INFO: RETURN: DriverPackagePreinstallW (0xE000024B) INFO: Preinstalling 'c:\program files (x86)\texas instruments\ads8350evm\sdcc driver\ti_usb-wv5.inf' ... INFO: ENTER: DriverPackagePreinstallW INFO: RETURN: DriverPackagePreinstallW (0xE0000247)
I can repeat over and over by running the
"c:\Program Files (x86)\Texas Instruments\ADS8350evm\SDCC Driver\driverInstall.exe"
I understand that this EVM is a bit "weathered" but this is what I got from TI today since there doesn't seem to be anything more current.
The issue seems to have same symptoms as the one described below by Oba-san in 2018 but I do not see resolution.
Thanks - Martin