Part Number: ADS8166
Other Parts Discussed in Thread: PGA281, , ADS8867, ADS8924B
Hi support forum
Question1: For the ADS8166 please look the attached design proposal and make a sanity check and let me know if there is any problem to use just one pair of MUX inputs for the PGA281 differential output signal?
Question2: ADS8166 pin20 ADS-INM, pin17 ADS-INP or is it better to connect the Diff. output from the PGA281 directly to these two inputs and avoiding the MUX in the ADC?
Question3: Or if it is a better choice to go for the ADS8867.
Question4: Are there any recommendation in parts selection for the 10y production in order to avoided any EOL situation?
Br Jørgen Lundbeck
Attachment: 810.009.250MS-01 AIM 2200 Measurement System.docx