This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1293: ADS1293 9-lead LOD application without RLD

Part Number: ADS1293

Hi TI member ,

Any update info ?

What the ADS1293 impedance of this path must be less the comparator threshold ?  

THX

  • Hi Wei,

    I have discussed this with the team, and the noise issue seems to affect the V-leads that are measured with respect to the WCT signal. It is not affecting the L-I or L-II in either test condition. The noise may be coupling from the WCT signal when the AC leadoff is enable. However, the AFE_1’s V1-lead does not seem to be affected even when the AFE_1 AC leadoff is enabled. I have listed some tests below to help better understand the issue.  

    1. Adding 100pF capacitor to the WCT pin to help filter the noise for the V-leads.
    2. Check the V-lead signal by disabling the AFE_1 AC-leadoff and enable the AFE_2 AC-leadoff.

    What the ADS1293 impedance of this path must be less the comparator threshold ?  

    I'm not sure what you means by this question. Can you please help to clarify? Please also reach out to the AFEs support at ads129x-support@list.ti.com for further support for the ADS1293.

    Thanks.

    -TC