Part Number: ADS1261
Bryan
As from our previous conversations, I'm sampling at 7200sps in continuous mode and using the SINC3 filtering. When using the ADS1261 Design Calculator spreadsheet (Digital Filter tab), I see that the initial settling time is .84ms for the first conversion and .14ms there after. When does the settling time start? After the last register write or after the start signal? Again, I'm acquiring two channels. The first channel will be sampled once, then the second channel will be sampled 10 time. I assume I'll have to wait the .84ms for the first channel. Again, I assume the first sample of the second channel will also require a wait time of .84ms. But considering that I'm running in continuous mode, should I use the MODE1 register to set a conversion start delay to lets say .189ms or can I collect the data as it comes on every DRDY?