This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I need to understand HBM ESD rating for the following fdevices:
TLV1548QDBREP
If not exact information is available please provide approximate based on process technology and device family.
Thank you,
HSG
Hello,
The ESD information we found is that this family was tested to the following levels without issue:
HBM: 2kV
CDM: 1kV
MM: 200V