This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299EEGFE-PDK: Compile and run the source code of the motherboard (DSP)

Part Number: ADS1299EEGFE-PDK

Hi team,

Our customers are trying to compile and run the source code (available on the official website) for the ADS1299EEGFE-PDK motherboard. The environment they use is CCS v5.5 and the BIOS driver is 5.42.2.10, but CCS can get a lot of errors. Most of the associated library files are perceived to be missing. The question I want to ask is what environment the official source code needs to run in, such as which version of CCS works, and where the missing related library files can be found. The errors reported by CCS after compilation are as follows

Best Regards,

Amy