Part Number: DAC8771
Other Parts Discussed in Thread: DAC8775
Hi DAC team,
Customer have question about a behavior when output is open. This is related to below link.
Your team mentioned "when the load is open in current output mode the voltage will increase in an attempt to drive the current to around 22V in full tracking mode."
If the alarm actio register is set to '01', I don't understand why the output voltage stop to increase around 22V. If no action is taken internally, I think output voltage increase as high as possible and it'll be broken. Also the value of 22V isn't shown on anywhere of the datasheet, is it correct value?
Would you let me know a behavior happen when output load goes to open?
In addition, is the DAC8771 going to be damaged if no action is taken after the output voltage keeps 22V?
Best regards,
Hideki