Part Number: ADS8691
Dear expert,
May I learn from you about how to read register value of bit[0:15]?
I only find <Read_HWORD> comment from datasheet table5.
Thanks.
Regards,
Ben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ben,
Here is an example to use READ_HWORD command to read the 16-bit of ALARM_H_TH_REG Register:
(Byte 0 Address for bits 7-0 = 24h, Byte 1 Address for bits 15-8 = 25h, Byte 2 Address for bits 23-16 = 26h, Byte 3 Address for bits 31-24 = 27h)
Data frame: <11001_xx> <0_0010_0100><00000000><00000000>
Data frame: <11001_xx> <0_0010_0110><00000000><00000000>
Please note:
Thanks®ards,
Dale