Other Parts Discussed in Thread: ADS7223
Hi.
My customer want to use ADS7223 on Single Input.
Then, is it possible to achieve resolution of 12 bit under the following condition?
- Fully differential mode
- Input Voltage = 0 ~ 3.3V
- VREF = 1.65V
- Input Voltage and VREF are inputted to CHxxP terminal and CHxxN terminal.
If there is short information, please point it out.
Kuramochi