This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
My customer want to use ADS7223 on Single Input.
Then, is it possible to achieve resolution of 12 bit under the following condition?
- Fully differential mode
- Input Voltage = 0 ~ 3.3V
- VREF = 1.65V
- Input Voltage and VREF are inputted to CHxxP terminal and CHxxN terminal.
If there is short information, please point it out.
Kuramochi
Hi Kuramochi,
Yes, if you use the 1.65V reference as one of the inputs (to CHxxN for instance) and apply your 0-3.3V signal to the other input, you would be taking a differential measurement between the two. I don't see any reason why you would have any issues reaching 12-bit resolution with the ADS7223. I would suggest that you consider buffering the reference before running it to the input.